Resources
Filter by
![](https://www.xppower.com/storage/resources/images/video/gsp500_video.jpg)
GSP500 series: Low noise, forced-cooled power supplies
Highly efficient GSP500 series power supply which provides 500 Watts forced-cooled or 180 Watts convection-cooled power...
![](https://www.xppower.com/storage/resources/images/blog/Power-60VDC_EMH250-3501114.jpg)
Power supply applications with output voltages exceeding 60VDC
Most commercially available power supplies have output voltages ranging from 3V3 to 54VDC. However, there are many end...
![](https://www.xppower.com/storage/resources/images/blog/ASB110_1.jpg)
Low profile full brick baseplate cooled AC-DC power supplies require no external components
XP Power’s ASB110 series provides a complete baseplate-cooled AC-DC power supply module that requires no external compon...
![](https://www.xppower.com/storage/resources/images/video/nanoflex_video.jpg)
nanofleX series: Configurable, digitally controlled AC-DC power supplies
XP Power today announced the nanofleX series of configurable digitally controlled AC-DC power supplies. This modular sup...
![](https://www.xppower.com/storage/resources/images/blog/Isolation.jpg)
Understanding Isolation Ratings in High Voltage Power Supplies
“My 10 kV power supply has an isolation rating of only 3500V, why is that?” This is a common initial reaction when revi...
![](https://www.xppower.com/storage/resources/images/blog/reliability-terms.jpg)
Reliability Terminology - Power Supplies
Failure Rate λ Failure rate is defined as the percentage of units failing per unit time. This varies throughout the...
![](https://www.xppower.com/storage/resources/images/blog/Understanding Energy Efficiency_1.jpg)
Energy efficiency for external power supplies (EPS)
Energy efficiency legislation is now in place across most regions of the world. In the main, the focus of these regulati...
![](https://www.xppower.com/storage/resources/images/blog/green_llc.jpg)
Green mode LLC half bridge converters
Power supplies marketed under the “Green” label are designed to maximise efficiency across the load range (average activ...
![](https://www.xppower.com/storage/resources/images/video/cch400_video.jpg)
Baseplate cooled, CCH400-600 series of power supplies
Meet compliance with both industry and military-grade approvals. They operate over a wide temperature range and feature...
![](https://www.xppower.com/storage/resources/images/blog/system_emi.jpg)
Determine System EMI Characteristics Early in System Design Phase
Often in the commercial, industrial, medical and military industries, system engineers wait until system qualification b...
![](https://www.xppower.com/storage/resources/images/video/ecp180_video.jpg)
ECP180 series of power supplies
120 Watts with convection-cooling and 180 Watts with force-cooling, all in a 2 x 4 x 1" package.
![](https://www.xppower.com/storage/resources/images/blog/MIL-STD-1275.jpg)
MIL-STD-1275 Compliance for power systems made easy.
The US Department of Defense Standard MIL-STD 1275 is an immunity standard that defines a series of test conditions to b...